Rescaling in the Graphs application affects only the graphs, plots, and objects that reside in the Graphing view. It has no effect on objects in the underlying Plane Geometry view.
▶ | To rescale the x and y axes proportionally, drag a tic mark on either axis. |
▶ | To rescale only one axis, hold down Shift and drag a tic mark on the axis. |
▶ | From the Window / Zoom menu, select one of the tools. |
- | Zoom - Box (Click two corners of a box to define the area to show.) |
- | Zoom - In |
- | Zoom - Out |
▶ | From the Window / Zoom menu, select one of the predefined Zoom settings. |
- | Zoom - Standard |
- | Zoom - Quadrant 1 |
- | Zoom - Standard User |
- | Zoom - Standard Trig |
- | Zoom - Standard Data |
- | Zoom - Fit |
1. | From the Window / Zoom menu, select Window Settings. |
2. | Enter a value for each setting. You can use expressions for exact input, as shown below. |
|
On TI‑Nspire™ products, fractional input is preserved as-is. Other exact inputs are replaced with the evaluated result. |
|
On TI‑Nspire™ CAS products, fractional and other exact inputs are preserved. |