You are here: Geometry Application > Creating Shapes Using Gestures (MathDraw)

Creating Shapes Using Gestures (MathDraw)

The MathDraw tool lets you use touchscreen or mouse gestures to create points, lines, circles, and other shapes.

MathDraw is available in:

Geometry view without the analytic window displayed.
Graphing view when the x scale and y scale are identical. This avoids non-circular ellipses and non-square rectangles appearing as circles and squares.

MathDraw is not available in the 3D Graphing view or in the Geometry view with the analytic window displayed.

Activating MathDraw

1. If using the Geometry view with the analytic window visible, use the View menu to hide the window.
2. On the Actions menu, select MathDraw.

The MathDraw icon appears. You can begin using the tool.

Canceling MathDraw

When you have finished using the MathDraw tool, press Esc.

The tool also closes if you select a different tool or change views.

ClosedCreating Points
ClosedDrawing Lines and Segments
ClosedDrawing Circles and Ellipses
ClosedDrawing Triangles
ClosedDrawing Rectangles and Squares
ClosedDrawing Polygons
ClosedUsing MathDraw to Create Equations
ClosedUsing MathDraw to Measure an Angle
ClosedUsing MathDraw to Find a Mid-point
ClosedUsing MathDraw to Erase

 

© 2006 - 2016 Texas Instruments Incorporated