You are here: Graphs Application > Using the Text Tool to Graph Equations
Using the Text Tool to Graph Equations
You can graph an "x=" or "y=" equation by typing it into a text box and dragging the text to an axis. You can edit the equation text (for example, change it to an inequality), but you cannot change it between x= and y=.
Graphing a Trigonometry Relation from Text
1.
From the Actions menu, select Text.
2.
Click the work area to place the text box.
3.
Type the equation for the trigonometry relation, such as x=sin(y)*2.
4.
Press Enter to complete the text object.
5.
Drag the text object to either axis to graph the equation.
Graphing a Vertical or Horizontal Line from Text
1.
From the Actions menu, select Text.
2.
Click the work area to place the text box.
3.
Type the equation for a vertical line, such as x=4, or a horizontal line, such as y=‑2. Click Enter to complete it.
4.
Drag the text object to either axis to graph the equation.
After plotting a line, you can drag to translate or rotate it.
Graphing an Inequality from Text
You can graph inequalities that use the >, <, ≤, or ≥ operators. Areas that satisfy the inequality are shown with shading. If the shaded areas of two or more inequalities overlap, the area of overlap is shaded darker.
1.
From the Actions menu, select Text.
2.
Click the work area to place the text box.
3.
Type the inequality expression, such as x<2*sin(y). Click Enter to complete it.
4.
Drag the text object to either axis to graph the inequality.