1. | (Optional) Create two predefined list variables containing the x and y values to plot. You can use the Lists & Spreadsheet, Calculator, or Notes application to create the lists. |
2. | From the Graph Entry/Edit menu, select Scatter Plot. |
Use the up and down arrow keys to move between the x and y fields.
3. | Use one of the following methods to specify lists to plot as x and y. |
- | Click to select names of the predefined list variables. |
- | Type the names of the variables, such as v1. |
- | Type lists as comma-separated elements enclosed within brackets, for example: {1,2,3}. |
4. | Press Enter to plot the data, and then zoom the work area to view the plotted data. |