You must store a function or program to make it accessible. The Program Editor automatically checks the syntax before storing. An asterisk (*) before the program or function name indicates that it has not been stored. To store a function or program:
1. | From the Program Editor, tap Tools and go to Check Syntax and Store. |
2. | Tap Check Syntax & Store. |
Program Editor checks for syntax errors and stores the program.
• | If no syntax errors are found, the message "stored successfully" is displayed in the status line after the program or function name. |
• | If syntax errors are found, an error message is displayed and the cursor is positioned near the first error. |
• | If the function or program is defined as a library object, you must also save the document in the designated library folder and refresh libraries to make the function or program accessible to other documents. |