Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Program Editor Overview > Accessing the Program Editor

Accessing the Program Editor

Program Editor is accessible from the Calculator application.

1. Open a document with the Calculator application active.
2. Tap Tools and go to Functions and Programs.
3. Tap Program Editor.

Options enable you to define a new program, open an existing program, or import a program from the Library.

4. Tap an option, complete the required information, and then tap OK.

The Program Editor opens with the selected template active on the right side of the screen.

 

Calculator work area. Tap the left side of the screen to return to and work in the Calculator application.

 

Program Editor work area. This is the default work area when Program Editor opens. If the Program Editor is not active, tap the right side of the screen.

 

Status line. Shows the line number information and the name of the function or program being defined or edited. An asterisk (*) indicates that this function has been changed since the last time syntax was checked and the function was stored.

 

 

© 2013 Texas Instruments Incorporated