1. | In the Graphs application, tap Tools ![]() |
2. | Use one of the following methods to specify two lists to plot as x and y. |
- | Tap ![]() |
- | Type the name of an existing list variable, such as v1. |
- | Type the list elements directly (for example, type {1,2,3}. |
3. | Tap ENTER to plot the data, and then zoom the work area to view the plotted data. |