| 1. | In the Graphs application, tap Tools and go to Graph Entry/Edit > Scatter Plot. |
| 2. | Use one of the following methods to specify two lists to plot as x and y. |
| - | Tap to select a list variable that you have defined in the current problem. |
| - | Type the name of an existing list variable, such as v1. |
| - | Type the list elements directly (for example, type {1,2,3}. |
| 3. | Tap ENTER to plot the data, and then zoom the work area to view the plotted data. |