|
ODE entry line:
|
||||||||||||
|
Slider added for adjusting coefficient k of the ODE |
||||||||||||
|
Slope field |
||||||||||||
|
A solution curve passing through the initial condition |
1. | In the Graphing view, tap Tools ![]() |
The ODE is automatically assigned an identifier, such as “y1.”
2. | Move to the relation field and enter the expression that defines the relation. For example, you might enter -y1+0.1*y1*y2. |
3. | Enter the initial condition for the independent value x0 and for y10. |
Note: The x0 value(s) are common to all the ODEs in a problem but can be entered or modified only in the first ODE.
4. | Tap Edit Parameters ![]() |
5. | Tap OK. |
6. | Zoom the window as necesssary to view the graph. |