self = physics.Space:setSleepTimeThreshold(sleep)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Space |
The input simulation Space |
|
sleep |
in number |
The amount of time (seconds) below which time if a Shape has not moved, it is put to sleep |
|
self |
out physics.Space |
The input Space is returned as the output |
Sleep time threshold is used to calculate when a Body can be put to sleep
Introduced in platform.apiLevel = '2.0'