self = physics.Space:setIdleSpeedThreshold(speed)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Space |
The input simulation Space |
|
speed |
in number |
Threshold speed |
|
self |
out physics.Space |
The input Space is returned as the output |
The idleSpeedThreshold is the speed below which a body is considered to be idle. This value is used to determine when a body can be put to sleep.
Introduced in platform.apiLevel = '2.0'