Damping drains speed from bodies in the simulation. A value of 0.9 means that each body will lose 10% of its speed per second. Defaults to 1. This value can be overridden on a per body basis.
self = physics.Space:setDamping(d)
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Space |
The input simulation Space |
|
d |
in number |
The new amount of damping for the simulation Space |
|
self |
out physics.Space |
The input Space is returned as the output |
Amount of viscous damping to apply to the Space.
Note
May not behave as expected for d larger than 1.0 or less than 0.
Introduced in platform.apiLevel = '2.0'