You are here:TI‑Nspire™/TI‑Nspire™ CX Reference Guide > T

T

T (transpose)

Matrix1T matrix

Returns the complex conjugate transpose of Matrix1.

Note: You can insert this operator from the computer keyboard by typing @t.

tan()


tan(Value1) value
tan(List1) list

tan(Value1) returns the tangent of the argument.

tan(List1) returns a list of the tangents of all elements in List1.

Note: The argument is interpreted as a degree, gradian or radian angle, according to the current angle mode. You can use °g or r to override the angle mode setting temporarily.

In Degree angle mode:


In Gradian angle mode:


In Radian angle mode:

tan(squareMatrix1) squareMatrix

Returns the matrix tangent of squareMatrix1. This is not the same as calculating the tangent of each element. For information about the calculation method, refer to cos().

squareMatrix1 must be diagonalizable. The result always contains floating-point numbers.

In Radian angle mode:

tan¹()

tan¹(Value1) value

tan¹(List1) list

tan¹(Value1) returns the angle whose tangent is Value1.

tan¹(List1) returns a list of the inverse tangents of each element of List1.

Note: The result is returned as a degree, gradian or radian angle, according to the current angle mode setting.

Note: You can insert this function from the keyboard by typing arctan(...).

In Degree angle mode:


In Gradian angle mode:


In Radian angle mode:

tan¹(squareMatrix1) squareMatrix

Returns the matrix inverse tangent of squareMatrix1. This is not the same as calculating the inverse tangent of each element. For information about the calculation method, refer to cos().

squareMatrix1 must be diagonalizable. The result always contains floating-point numbers.

In Radian angle mode:

tanh()

tanh(Value1) value

tanh(List1) list

tanh(Value1) returns the hyperbolic tangent of the argument.

tanh(List1) returns a list of the hyperbolic tangents of each element of List1.

tanh(squareMatrix1) squareMatrix

Returns the matrix hyperbolic tangent of squareMatrix1. This is not the same as calculating the hyperbolic tangent of each element. For information about the calculation method, refer to cos().

squareMatrix1 must be diagonalizable. The result always contains floating-point numbers.

In Radian angle mode:

tanh¹()


tanh¹(Value1) value
tanh¹(List1) list

tanh¹(Value1) returns the inverse hyperbolic tangent of the argument.

tanh¹(List1) returns a list of the inverse hyperbolic tangents of each element of List1.

Note: You can insert this function from the keyboard by typing arctanh(...).

In Rectangular complex format:

To see the entire result, press £ and then use ¡ and ¢ to move the cursor.

tanh¹(squareMatrix1) squareMatrix

Returns the matrix inverse hyperbolic tangent of squareMatrix1. This is not the same as calculating the inverse hyperbolic tangent of each element. For information about the calculation method, refer to cos().

squareMatrix1 must be diagonalizable. The result always contains floating-point numbers.

In Radian angle mode and Rectangular complex format:

To see the entire result, press £ and then use ¡ and ¢ to move the cursor.

tCdf()

tCdf(lowBound,upBound,df) number if lowBound and upBound are numbers, list if lowBound and upBound are lists

Computes the Student-t distribution probability between lowBound and upBound for the specified degrees of freedom df.

For P(X upBound), set lowBound = 9E999.

 

Text

TextpromptString[, DispFlag]

Programming command: Pauses the program and displays the character string promptString in a dialog box.

When the user selects OK, program execution continues.

The optional flag argument can be any expression.

If DispFlag is omitted or evaluates to 1, the text message is added to the Calculator history.
If DispFlag evaluates to 0, the text message is not added to the history.

If the program needs a typed response from the user, refer to Request, here, or RequestStr, here.

Note: You can use this command within a user-defined program but not within a function.

Define a program that pauses to display each of five random numbers in a dialog box.

Within the Prgm...EndPrgm template, complete each line by pressing @ instead of ·. On the computer keyboard, hold down Alt and press Enter.

 

Define text_demo()=Prgm
  For i,1,5
    strinfo:=”Random number “ & string(rand(i))
    Text strinfo
  EndFor
EndPrgm

 

Run the program:

text_demo()

 

Sample of one dialog box:

Then

 

 

tInterval

tInterval List[, Freq[, CLevel]]

(Data list input)

tInterval v, sx, n[, CLevel]

(Summary stats input)

Computes a t confidence interval. A summary of results is stored in the stat.results variable. (See here.)

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.CLower, stat.CUpper

Confidence interval for an unknown population mean

stat.v

Sample mean of the data sequence from the normal random distribution

stat.ME

Margin of error

stat.df

Degrees of freedom

stat.σx

Sample standard deviation

stat.n

Length of the data sequence with sample mean

tInterval_2Samp

tInterval_2Samp List1,List2[,Freq1[,Freq2[,CLevel[,Pooled]]]]

(Data list input)

tInterval_2Samp v1,sx1,n1,v2,sx2,n2[,CLevel[,Pooled]]

(Summary stats input)

Computes a two-sample t confidence interval. A summary of results is stored in the stat.results variable. (See here.)

Pooled=1 pools variances; Pooled=0 does not pool variances.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.CLower, stat.CUpper

Confidence interval containing confidence level probability of distribution

stat.v1-v2

Sample means of the data sequences from the normal random distribution

stat.ME

Margin of error

stat.df

Degrees of freedom

stat.v1, stat.v2

Sample means of the data sequences from the normal random distribution

stat.σx1, stat.σx2

Sample standard deviations for List 1 and List 2

stat.n1, stat.n2

Number of samples in data sequences

stat.sp

The pooled standard deviation. Calculated when Pooled = YES

tPdf()

tPdf(XVal,df) number if XVal is a number, list if XVal is a list

Computes the probability density function (pdf) for the Student-t distribution at a specified x value with specified degrees of freedom df.

 

trace()

trace(squareMatrix) value

Returns the trace (sum of all the elements on the main diagonal) of squareMatrix.

Try

Try
     block1
Else
     block2
EndTry

Executes block1 unless an error occurs. Program execution transfers to block2 if an error occurs in block1. System variable errCode contains the error code to allow the program to perform error recovery. For a list of error codes, see “Error codes and messages,” here.

block1 and block2 can be either a single statement or a series of statements separated with the “:” character.

Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook.

To see the commands Try, ClrErr, and PassErr in operation, enter the eigenvals() program shown at the right. Run the program by executing each of the following expressions.

Note: See also ClrErr, here, and PassErr, here.

Define eigenvals(a,b)=Prgm
© Program eigenvals(A,B) displays eigenvalues of AB

Try
    Disp "A= ",a
    Disp "B= ",b
    Disp " "

    Disp "Eigenvalues of AB are:",eigVl(a*b)

Else
    If errCode=230 Then
        Disp "Error: Product of AB must be a square matrix"
        ClrErr
    Else
        PassErr
    EndIf
EndTry

EndPrgm

 

tTest

tTest μ0,List[,Freq[,Hypoth]]

(Data list input)

tTest μ0,v,sx,n,[Hypoth]

(Summary stats input)

Performs a hypothesis test for a single unknown population mean μ when the population standard deviation σ is unknown. A summary of results is stored in the stat.results variable. (See here.)

Test H0: μ = μ0, against one of the following:

For Ha: μ < μ0, set Hypoth<0
For Ha: μ μ0 (default), set Hypoth=0
For Ha: μ > μ0, set Hypoth>0

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.t

(v μ0) / (stdev / sqrt(n))

stat.PVal

Smallest level of significance at which the null hypothesis can be rejected

stat.df

Degrees of freedom

stat.v

Sample mean of the data sequence in List

stat.sx

Sample standard deviation of the data sequence

stat.n

Size of the sample

tTest_2Samp

tTest_2Samp List1,List2[,Freq1[,Freq2[,Hypoth[,Pooled]]]]

(Data list input)

tTest_2Samp v1,sx1,n1,v2,sx2,n2[,Hypoth[,Pooled]]

(Summary stats input)

Computes a two-sample t test. A summary of results is stored in the stat.results variable. (See here.)

Test H0: μ1 = μ2, against one of the following:

For Ha: μ1< μ2, set Hypoth<0
For Ha: μ1 μ2 (default), set Hypoth=0
For Ha: μ1> μ2, set Hypoth>0

Pooled=1 pools variances
Pooled=0 does not pool variances

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

Output variable

Description

stat.t

Standard normal value computed for the difference of means

stat.PVal

Smallest level of significance at which the null hypothesis can be rejected

stat.df

Degrees of freedom for the t-statistic

stat.v1, stat.v2

Sample means of the data sequences in List 1 and List 2

stat.sx1, stat.sx2

Sample standard deviations of the data sequences in List 1 and List 2

stat.n1, stat.n2

Size of the samples

stat.sp

The pooled standard deviation. Calculated when Pooled=1.

tvmFV()

tvmFV(N,I,PV,Pmt,[PpY],[CpY],[PmtAt]) value

Financial function that calculates the future value of money.

Note: Arguments used in the TVM functions are described in the table of TVM arguments, here. See also amortTbl(), here.

tvmI()

tvmI(N,PV,Pmt,FV,[PpY],[CpY],[PmtAt]) value

Financial function that calculates the interest rate per year.

Note: Arguments used in the TVM functions are described in the table of TVM arguments, here. See also amortTbl(), here.

tvmN()

tvmN(I,PV,Pmt,FV,[PpY],[CpY],[PmtAt]) value

Financial function that calculates the number of payment periods.

Note: Arguments used in the TVM functions are described in the table of TVM arguments, here. See also amortTbl(), here.

tvmPmt()

tvmPmt(N,I,PV,FV,[PpY],[CpY],[PmtAt]) value

Financial function that calculates the amount of each payment.

Note: Arguments used in the TVM functions are described in the table of TVM arguments, here. See also amortTbl(), here.

tvmPV()

tvmPV(N,I,Pmt,FV,[PpY],[CpY],[PmtAt]) value

Financial function that calculates the present value.

Note: Arguments used in the TVM functions are described in the table of TVM arguments, here. See also amortTbl(), here.

TVM argument*

Description

Data type

N

Number of payment periods

real number

I

Annual interest rate

real number

PV

Present value

real number

Pmt

Payment amount

real number

FV

Future value

real number

PpY

Payments per year, default=1

integer > 0

CpY

Compounding periods per year, default=1

integer > 0

PmtAt

Payment due at the end or beginning of each period, default=end

integer (0=end, 1=beginning)

* These time-value-of-money argument names are similar to the TVM variable names (such as tvm.pv and tvm.pmt) that are used by the Calculator application’s finance solver. Financial functions, however, do not store their argument values or results to the TVM variables.

TwoVar

TwoVar X, Y[, [Freq][, Category, Include]]

Calculates the TwoVar statistics. A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension except for Include.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Category is a list of numeric category codes for the corresponding X and Y data.

Include is a list of one or more of the category codes. Only those data items whose category code is included in this list are included in the calculation.

An empty (void) element in any of the lists X, Freq, or Category results in a void for the corresponding element of all those lists. An empty element in any of the lists X1 through X20 results in a void for the corresponding element of all those lists. For more information on empty elements, see here.

 

Output variable

Description

stat.v

Mean of x values

stat.Σx

Sum of x values

stat.Σx2

Sum of x2 values

stat.sx

Sample standard deviation of x

stat.σx

Population standard deviation of x

stat.n

Number of data points

stat.w

Mean of y values

stat.Σy

Sum of y values

stat.Σy2

Sum of y2 values

stat.sy

Sample standard deviation of y

stat.σy

Population standard deviation of y

stat.Σxy

Sum of xy values

stat.r

Correlation coefficient

stat.MinX

Minimum of x values

stat.Q1X

1st Quartile of x

stat.MedianX

Median of x

stat.Q3X

3rd Quartile of x

stat.MaxX

Maximum of x values

stat.MinY

Minimum of y values

stat.Q1Y

1st Quartile of y

stat.MedY

Median of y

stat.Q3Y

3rd Quartile of y

stat.MaxY

Maximum of y values

stat.Σ(x-v)2

Sum of squares of deviations from the mean of x

stat.Σ(y-w)2

Sum of squares of deviations from the mean of y