You are here:TI‑Nspire™/TI‑Nspire™ CX Reference Guide > A

A

abs()


abs(Value1) value
abs(List1) list
abs(Matrix1) matrix

Returns the absolute value of the argument.

Note: See also Absolute value template, here.

If the argument is a complex number, returns the number’s modulus.

amortTbl()

amortTbl(NPmt,N,I,PV, [Pmt], [FV], [PpY], [CpY], [PmtAt], [roundValue]) matrix

Amortization function that returns a matrix as an amortization table for a set of TVM arguments.

NPmt is the number of payments to be included in the table. The table starts with the first payment.

N, I, PV, Pmt, FV, PpY, CpY, and PmtAt are described in the table of TVM arguments, here.

If you omit Pmt, it defaults to Pmt=tvmPmt(N,I,PV,FV,PpY,CpY,PmtAt).
If you omit FV, it defaults to FV=0.
The defaults for PpY, CpY, and PmtAt are the same as for the TVM functions.

roundValue specifies the number of decimal places for rounding. Default=2.

The columns in the result matrix are in this order: Payment number, amount paid to interest, amount paid to principal, and balance.

The balance displayed in row n is the balance after payment n.

You can use the output matrix as input for the other amortization functions ΣInt() and ΣPrn(), here, and bal(), here.

and

BooleanExpr1 and BooleanExpr2 Boolean expression

BooleanList1 and BooleanList2 Boolean list

BooleanMatrix1 and BooleanMatrix2 Boolean matrix

Returns true or false or a simplified form of the original entry.

Integer1 andInteger2 integer

Compares two real integers bit-by-bit using an and operation. Internally, both integers are converted to signed, 64-bit binary numbers. When corresponding bits are compared, the result is 1 if both bits are 1; otherwise, the result is 0. The returned value represents the bit results, and is displayed according to the Base mode.

You can enter the integers in any number base. For a binary or hexadecimal entry, you must use the 0b or 0h prefix, respectively. Without a prefix, integers are treated as decimal (base 10).

In Hex base mode:

Important: Zero, not the letter O.


In Bin base mode:


In Dec base mode:

Note: A binary entry can have up to 64 digits (not counting the 0b prefix). A hexadecimal entry can have up to 16 digits.

angle()

angle(Value1) value

Returns the angle of the argument, interpreting the argument as a complex number.

In Degree angle mode:


In Gradian angle mode:


In Radian angle mode:

angle(List1) list
angle(Matrix1) matrix

Returns a list or matrix of angles of the elements in List1 or Matrix1, interpreting each element as a complex number that represents a two-dimensional rectangular coordinate point.

ANOVA

ANOVA List1,List2[,List3,...,List20][,Flag]

Performs a one-way analysis of variance for comparing the means of two to 20 populations. A summary of results is stored in the stat.results variable. (here)

Flag=0 for Data, Flag=1 for Stats

 

 

Output variable

Description

stat.F

Value of the F statistic

stat.PVal

Smallest level of significance at which the null hypothesis can be rejected

stat.df

Degrees of freedom of the groups

stat.SS

Sum of squares of the groups

stat.MS

Mean squares for the groups

stat.dfError

Degrees of freedom of the errors

stat.SSError

Sum of squares of the errors

stat.MSError

Mean square for the errors

stat.sp

Pooled standard deviation

stat.xbarlist

Mean of the input of the lists

stat.CLowerList

95% confidence intervals for the mean of each input list

stat.CUpperList

95% confidence intervals for the mean of each input list

ANOVA2way

ANOVA2way List1,List2[,List3,,List10][,levRow]

Computes a two-way analysis of variance for comparing the means of two to 10 populations. A summary of results is stored in the stat.results variable. (See here.)

LevRow=0 for Block

LevRow=2,3,...,Len-1, for Two Factor, where Len=length(List1)=length(List2) = … = length(List10) and Len / LevRow  Π {2,3,…}

 

 

Outputs: Block Design

Output variable

Description

stat.F

F statistic of the column factor

stat.PVal

Smallest level of significance at which the null hypothesis can be rejected

stat.df

Degrees of freedom of the column factor

stat.SS

Sum of squares of the column factor

stat.MS

Mean squares for column factor

stat.FBlock

F statistic for factor

stat.PValBlock

Least probability at which the null hypothesis can be rejected

stat.dfBlock

Degrees of freedom for factor

stat.SSBlock

Sum of squares for factor

stat.MSBlock

Mean squares for factor

stat.dfError

Degrees of freedom of the errors

stat.SSError

Sum of squares of the errors

stat.MSError

Mean squares for the errors

stat.s

Standard deviation of the error

COLUMN FACTOR Outputs

Output variable

Description

stat.Fcol

F statistic of the column factor

stat.PValCol

Probability value of the column factor

stat.dfCol

Degrees of freedom of the column factor

stat.SSCol

Sum of squares of the column factor

stat.MSCol

Mean squares for column factor

ROW FACTOR Outputs

Output variable

Description

stat.FRow

F statistic of the row factor

stat.PValRow

Probability value of the row factor

stat.dfRow

Degrees of freedom of the row factor

stat.SSRow

Sum of squares of the row factor

stat.MSRow

Mean squares for row factor

INTERACTION Outputs

Output variable

Description

stat.FInteract

F statistic of the interaction

stat.PValInteract

Probability value of the interaction

stat.dfInteract

Degrees of freedom of the interaction

stat.SSInteract

Sum of squares of the interaction

stat.MSInteract

Mean squares for interaction

ERROR Outputs

Output variable

Description

stat.dfError

Degrees of freedom of the errors

stat.SSError

Sum of squares of the errors

stat.MSError

Mean squares for the errors

s

Standard deviation of the error

Ans

Ans value

Returns the result of the most recently evaluated expression.

approx()

approx(Value1) number

Returns the evaluation of the argument as an expression containing decimal values, when possible, regardless of the current Auto or Approximate mode.

This is equivalent to entering the argument and pressing /·.

approx(List1) list
approx(Matrix1) matrix

Returns a list or matrix where each element has been evaluated to a decimal value, when possible.

approxFraction()

ValueapproxFraction([Tol]) value

ListapproxFraction([Tol]) list

MatrixapproxFraction([Tol]) matrix

Returns the input as a fraction, using a tolerance of Tol. If Tol is omitted, a tolerance of 5.E-14 is used.

Note: You can insert this function from the computer keyboard by typing @>approxFraction(...).

approxRational()

approxRational(Value[, Tol]) value

approxRational(List[, Tol]) list

approxRational(Matrix[, Tol]) matrix

Returns the argument as a fraction using a tolerance of Tol. If Tol is omitted, a tolerance of 5.E-14 is used.

arccos()

 

 

arccosh()

 

 

arccot()

 

 

arccoth()

 

 

arccsc()

 

 

arccsch()

 

 

arcsec()

 

 

arcsech()

 

 

arcsin()

 

 

arcsinh()

 

 

arctan()

 

 

arctanh()

 

 

augment()

augment(List1, List2) list

Returns a new list that is List2 appended to the end of List1.

augment(Matrix1, Matrix2) matrix

Returns a new matrix that is Matrix2 appended to Matrix1. When the “,” character is used, the matrices must have equal row dimensions, and Matrix2 is appended to Matrix1 as new columns. Does not alter Matrix1 or Matrix2.

avgRC()

avgRC(Expr1, Var [=Value] [, Step]) expression

avgRC(Expr1, Var [=Value] [, List1]) list

avgRC(List1, Var [=Value] [, Step]) list

avgRC(Matrix1, Var [=Value] [, Step]) matrix

Returns the forward-difference quotient (average rate of change).

Expr1 can be a user-defined function name (see Func).

When Value is specified, it overrides any prior variable assignment or any current “|” substitution for the variable.

Step is the step value. If Step is omitted, it defaults to 0.001.

Note that the similar function centralDiff() uses the central-difference quotient.