Accessing the Program Editor
Program Editor is accessible from the Calculator application.
1. | Open a document with the Calculator ![]() |
2. | Tap Tools ![]() |
3. | Tap Program Editor. |
Options enable you to define a new program, open an existing program, or import a program from the Library.
4. | Tap an option, complete the required information, and then tap OK. |
The Program Editor opens with the selected template active on the right side of the screen.
|
|
Calculator work area. Tap the left side of the screen to return to and work in the Calculator application. |
|
|
Program Editor work area. This is the default work area when Program Editor opens. If the Program Editor is not active, tap the right side of the screen. |
|
|
Status line. Shows the line number information and the name of the function or program being defined or edited. An asterisk (*) indicates that this function has been changed since the last time syntax was checked and the function was stored. |