Entering Press-to-Test Mode with a Test Code

Note: This applies to TI-Nspire™ CX II handhelds only. You can obtain a test code by using the Choose Restrictions method or preparing the handheld in the TI-Nspire™ Premium Teacher software (see the Preparing Handhelds Remotely section in that guidebook).

1. Ensure that the handheld is turned off.
2. Press and hold down the e c keys.

Do not release the keys until the Enter Press-to-Test Code screen is displayed.

Note: This also displays after restoring factory defaults or rebooting the handheld.

3. Enter your eight-digit test code.

If the code is valid, a green checkmark will display.

Note: This example uses the TI Factory Default Code 0001-6382.

4. Press Next.

The Summary screen displays.

Scroll to review the restrictions or press Back to enter a different code.

5. Press Start to enter Press-to-Test mode.

After rebooting, the Summary screen displays.

6. Press OK to start the test.

Notes

• When the code is validated, it is stored and will be displayed when the Enter Press-to-Test Code dialog is invoked again.
• The same test codes are used for all TI-Nspire™ CX II CAS, TI-Nspire™ CX II and TI-Nspire™ CX II-T handhelds. The CAS and Exact Arithmetic Mode settings are ignored when appropriate.