Setting Up an Offline Sensor
You can predefine meter settings for a sensor that is not currently attached to a computer or handheld.
You cannot use the sensor offline, but you can prepare the experiment for it and then attach it when ready to collect the data. This option makes it faster to share a sensor during a lesson or lab in which there are not enough sensors for everyone.
| 1.
|
From the menu, select. |
The Select Sensor dialog box opens.
| 2.
|
Select a sensor from the list. |
| 3.
|
Click the tab . |
The settings will be applied when you attach the sensor.
Removing an offline sensor
| 1.
|
From the menu, select . |
| 2.
|
Select the name of the offline sensor to remove. |