Creating Geometric Objects
You can create objects in both the Geometry and Graphs applications.
Creating Points and Lines
|
1.
|
Tap , select , and select the type of object, such as . (In the Graphs application, go to .) |
|
2.
|
Tap existing points or locations on the work area to define the object. For example, tap two objects when creating Intersection points. |
As you create the object, a tool is shown in the application Toolbar (for example,
). To cancel, tap the on the tool.
Creating Geometric Shapes
|
1.
|
Tap , select , and select the type of object, such as . (In the Graphs application, go to .) |
|
2.
|
Tap existing points or locations on the work area to define the object. For example, tap two locations to define the center and radius of a circle. |
As you create a shape, a tool is shown in the application Toolbar (for example,
). To cancel the shape, tap the on the tool.