Creating Shapes Using Gestures (MathDraw)
The MathDraw tool lets you use touchscreen gestures to create points, lines, circles, and other shapes.
| • | MathDraw is available in Geometry and Graphing. |
| • | Graphing view when the x scale and y scale are identical. This avoids non-circular ellipses and non-square rectangles appearing as circles and squares. |
Note: MathDraw is not available in the 3D Graphing.
Activating MathDraw
| 1. | Tap Add, and then tap . |
| 2. | Tap Tools . |
| 3. | Tap Actions menu, select MathDraw. |
The MathDraw tool
appears in the application Toolbar. You can begin using the tool.
Canceling MathDraw
| ▶ | When you have finished using the MathDraw tool, tap the X on the tool. |
.
.
Creating Points