Error Codes and Messages
When an error occurs, its code is assigned to variable errCode. User-defined programs and functions can examine errCode to determine the cause of an error. For an example of using errCode, See Example 2 under the Try command, here.
Note: Some error conditions apply only to TI‑Nspire™ CAS products, and some apply only to TI‑Nspire™ products.
|
Error code |
Description |
||||||||||||
|
10 |
A function did not return a value |
||||||||||||
|
20 |
A test did not resolve to TRUE or FALSE. Generally, undefined variables cannot be compared. For example, the test If a<b will cause this error if either a or b is undefined when the If statement is executed. |
||||||||||||
|
30 |
Argument cannot be a folder name. |
||||||||||||
|
40 |
Argument error |
||||||||||||
|
50 |
Argument mismatch Two or more arguments must be of the same type. |
||||||||||||
|
60 |
Argument must be a Boolean expression or integer |
||||||||||||
|
70 |
Argument must be a decimal number |
||||||||||||
|
90 |
Argument must be a list |
||||||||||||
|
100 |
Argument must be a matrix |
||||||||||||
|
130 |
Argument must be a string |
||||||||||||
|
140 |
Argument must be a variable name. Make sure that the name:
See the Calculator section in the documentation for more details. |
||||||||||||
|
160 |
Argument must be an expression |
||||||||||||
|
165 |
Batteries too low for sending or receiving Install new batteries before sending or receiving. |
||||||||||||
|
170 |
Bound The lower bound must be less than the upper bound to define the search interval. |
||||||||||||
|
180 |
Break The d or c key was pressed during a long calculation or during program execution. |
||||||||||||
|
190 |
Circular definition This message is displayed to avoid running out of memory during infinite replacement of variable values during simplification. For example, a+1->a, where a is an undefined variable, will cause this error. |
||||||||||||
|
200 |
Constraint expression invalid For example, solve(3x^2-4=0,x) | x<0 or x>5 would produce this error message because the constraint is separated by “or” instead of “and.” |
||||||||||||
|
210 |
Invalid Data type An argument is of the wrong data type. |
||||||||||||
|
220 |
Dependent limit |
||||||||||||
|
230 |
Dimension A list or matrix index is not valid. For example, if the list {1,2,3,4} is stored in L1, then L1[5] is a dimension error because L1 only contains four elements. |
||||||||||||
|
235 |
Dimension Error. Not enough elements in the lists. |
||||||||||||
|
240 |
Dimension mismatch Two or more arguments must be of the same dimension. For example, [1,2]+[1,2,3] is a dimension mismatch because the matrices contain a different number of elements. |
||||||||||||
|
250 |
Divide by zero |
||||||||||||
|
260 |
Domain error An argument must be in a specified domain. For example, rand(0) is not valid. |
||||||||||||
|
270 |
Duplicate variable name |
||||||||||||
|
280 |
Else and ElseIf invalid outside of If...EndIf block |
||||||||||||
|
290 |
EndTry is missing the matching Else statement |
||||||||||||
|
295 |
Excessive iteration |
||||||||||||
|
300 |
Expected 2 or 3-element list or matrix |
||||||||||||
|
310 |
The first argument of nSolve must be an equation in a single variable. It cannot contain a non-valued variable other than the variable of interest. |
||||||||||||
|
320 |
First argument of solve or cSolve must be an equation or inequality For example, solve(3x^2-4,x) is invalid because the first argument is not an equation. |
||||||||||||
|
345 |
Inconsistent units |
||||||||||||
|
350 |
Index out of range |
||||||||||||
|
360 |
Indirection string is not a valid variable name |
||||||||||||
|
380 |
Undefined Ans Either the previous calculation did not create Ans, or no previous calculation was entered. |
||||||||||||
|
390 |
Invalid assignment |
||||||||||||
|
400 |
Invalid assignment value |
||||||||||||
|
410 |
Invalid command |
||||||||||||
|
430 |
Invalid for the current mode settings |
||||||||||||
|
435 |
Invalid guess |
||||||||||||
|
440 |
Invalid implied multiply For example, x(x+1) is invalid; whereas, x*(x+1) is the correct syntax. This is to avoid confusion between implied multiplication and function calls. |
||||||||||||
|
450 |
Invalid in a function or current expression Only certain commands are valid in a user-defined function. |
||||||||||||
|
490 |
Invalid in Try..EndTry block |
||||||||||||
|
510 |
Invalid list or matrix |
||||||||||||
|
550 |
Invalid outside function or program A number of commands are not valid outside a function or program. For example, Local cannot be used unless it is in a function or program. |
||||||||||||
|
560 |
Invalid outside Loop..EndLoop, For..EndFor, or While..EndWhile blocks For example, the Exit command is valid only inside these loop blocks. |
||||||||||||
|
565 |
Invalid outside program |
||||||||||||
|
570 |
Invalid pathname For example, \var is invalid. |
||||||||||||
|
575 |
Invalid polar complex |
||||||||||||
|
580 |
Invalid program reference Programs cannot be referenced within functions or expressions such as 1+p(x) where p is a program. |
||||||||||||
|
600 |
Invalid table |
||||||||||||
|
605 |
Invalid use of units |
||||||||||||
|
610 |
Invalid variable name in a Local statement |
||||||||||||
|
620 |
Invalid variable or function name |
||||||||||||
|
630 |
Invalid variable reference |
||||||||||||
|
640 |
Invalid vector syntax |
||||||||||||
|
650 |
Link transmission A transmission between two units was not completed. Verify that the connecting cable is connected firmly to both ends. |
||||||||||||
|
665 |
Matrix not diagonalizable |
||||||||||||
|
670 |
Low Memory 1. Delete some data in this document 2. Save and close this document If 1 and 2 fail, pull out and re-insert batteries |
||||||||||||
|
672 |
Resource exhaustion |
||||||||||||
|
673 |
Resource exhaustion |
||||||||||||
|
680 |
Missing ( |
||||||||||||
|
690 |
Missing ) |
||||||||||||
|
700 |
Missing “ |
||||||||||||
|
710 |
Missing ] |
||||||||||||
|
720 |
Missing } |
||||||||||||
|
730 |
Missing start or end of block syntax |
||||||||||||
|
740 |
Missing Then in the If..EndIf block |
||||||||||||
|
750 |
Name is not a function or program |
||||||||||||
|
765 |
No functions selected |
||||||||||||
|
780 |
No solution found |
||||||||||||
|
800 |
Non-real result For example, if the software is in the Real setting, √(-1) is invalid. To allow complex results, change the “Real or Complex” Mode Setting to RECTANGULAR or POLAR. |
||||||||||||
|
830 |
Overflow |
||||||||||||
|
850 |
Program not found A program reference inside another program could not be found in the provided path during execution. |
||||||||||||
|
855 |
Rand type functions not allowed in graphing |
||||||||||||
|
860 |
Recursion too deep |
||||||||||||
|
870 |
Reserved name or system variable |
||||||||||||
|
900 |
Argument error Median-median model could not be applied to data set. |
||||||||||||
|
910 |
Syntax error |
||||||||||||
|
920 |
Text not found |
||||||||||||
|
930 |
Too few arguments The function or command is missing one or more arguments. |
||||||||||||
|
940 |
Too many arguments The expression or equation contains an excessive number of arguments and cannot be evaluated. |
||||||||||||
|
950 |
Too many subscripts |
||||||||||||
|
955 |
Too many undefined variables |
||||||||||||
|
960 |
Variable is not defined No value is assigned to variable. Use one of the following commands:
to assign values to variables. |
||||||||||||
|
965 |
Unlicensed OS |
||||||||||||
|
970 |
Variable in use so references or changes are not allowed |
||||||||||||
|
980 |
Variable is protected |
||||||||||||
|
990 |
Invalid variable name Make sure that the name does not exceed the length limitations |
||||||||||||
|
1000 |
Window variables domain |
||||||||||||
|
1010 |
Zoom |
||||||||||||
|
1020 |
Internal error |
||||||||||||
|
1030 |
Protected memory violation |
||||||||||||
|
1040 |
Unsupported function. This function requires Computer Algebra System. Try TI‑Nspire™ CAS. |
||||||||||||
|
1045 |
Unsupported operator. This operator requires Computer Algebra System. Try TI‑Nspire™ CAS. |
||||||||||||
|
1050 |
Unsupported feature. This operator requires Computer Algebra System. Try TI‑Nspire™ CAS. |
||||||||||||
|
1060 |
Input argument must be numeric. Only inputs containing numeric values are allowed. |
||||||||||||
|
1070 |
Trig function argument too big for accurate reduction |
||||||||||||
|
1080 |
Unsupported use of Ans.This application does not support Ans. |
||||||||||||
|
1090 |
Function is not defined. Use one of the following commands:
to define a function. |
||||||||||||
|
1100 |
Non-real calculation For example, if the software is in the Real setting, √(-1) is invalid. To allow complex results, change the “Real or Complex” Mode Setting to RECTANGULAR or POLAR. |
||||||||||||
|
1110 |
Invalid bounds |
||||||||||||
|
1120 |
No sign change |
||||||||||||
|
1130 |
Argument cannot be a list or matrix |
||||||||||||
|
1140 |
Argument error The first argument must be a polynomial expression in the second argument. If the second argument is omitted, the software attempts to select a default. |
||||||||||||
|
1150 |
Argument error The first two arguments must be polynomial expressions in the third argument. If the third argument is omitted, the software attempts to select a default. |
||||||||||||
|
1160 |
Invalid library pathname A pathname must be in the form xxx\yyy, where:
See the Library section in the documentation for more details. |
||||||||||||
|
1170 |
Invalid use of library pathname
|
||||||||||||
|
1180 |
Invalid library variable name. Make sure that the name:
See the Library section in the documentation for more details. |
||||||||||||
|
1190 |
Library document not found:
See the Library section in the documentation for more details. |
||||||||||||
|
1200 |
Library variable not found:
See the Library section in the documentation for more details. |
||||||||||||
|
1210 |
Invalid library shortcut name. Make sure that the name:
See the Library section in the documentation for more details. |
||||||||||||
|
1220 |
Domain error: The tangentLine and normalLine functions support real-valued functions only. |
||||||||||||
|
1230 |
Domain error. Trigonometric conversion operators are not supported in Degree or Gradian angle modes. |
||||||||||||
|
1250 |
Argument Error Use a system of linear equations. Example of a system of two linear equations with variables x and y: 3x+7y=5 2y-5x=-1 |
||||||||||||
|
1260 |
Argument Error: The first argument of |
||||||||||||
|
1270 |
Argument Error Order of the derivative must be equal to 1 or 2. |
||||||||||||
|
1280 |
Argument Error Use a polynomial in expanded form in one variable. |
||||||||||||
|
1290 |
Argument Error Use a polynomial in one variable. |
||||||||||||
|
1300 |
Argument Error The coefficients of the polynomial must evaluate to numeric values. |
||||||||||||
|
1310 |
Argument error: A function could not be evaluated for one or more of its arguments. |
||||||||||||
|
1380 |
Argument error: Nested calls to domain() function are not allowed. |