The Python App contains menus of functions, classes, controls, operators and keywords for quick pasting in the Editor or Shell. The following reference table contains the listing of features in y N when the App is running. For a complete listing of Python functions, classes, operators, and keywords available in this version, please see "Selected TI-Python Built-in, Keywords, and Module Content."
This table is not intended to be an exhaustive list of Python available in this offering. Other functions supported in this Python offering can be entered using the alpha keys from the keypad.
Most examples given in this table run at the Shell prompt (>>>).