The SmartPad™ CE App is available for the TI-84 Plus CE. To use the TI-84 Plus CE as a remote keypad for TI-SmartView™ CE:
1.
SmartPad™ CE App for TI-84 Plus CE comes pre-loaded on the calculator. If not on your TI-84 Plus CE, SmartPad CE App is also available to load to your calculator at education.ti.com/84ceupdate.
2.
Connect your TI-84 Plus CE to your computer using a USB Computer cable which came with your calculator.
3.
Launch TI-SmartView™ CE. Make sure the TI-SmartView™ CE window is in focus by clicking on the TI-SmartView™ CE window.
4.
Run SmartPad™ CE App on your TI-84 Plus CE. Press [apps] and select SmartPad™ CE from the Apps menu. Read the information on the splash screen.
5.
Press keys on the calculator's keypad which remotely press the emulator keypad on the TI-SmartView™ CE.
6.
Disconnect USB cable from calculator to stop the App and remote keypad feature.
7.
Reconnecting the USB cable and running the App again may be needed if the remote keypad connectivity is no longer responding.
Notes:
•
The TI-84 Plus CE running the SmartPad™ CE App will not display the calculations or graphs. The calculator becomes a remote USB keypad for the emulator only.
•
The TI-84 Plus CE will remain a remote keypad when the TI-SmartView™ CE window is in focus. Click on the TI-SmartView™ CE window prior to pressing keys on the calculator.
•
The TI SilverLink cable is not supported in TI-SmartView™ CE.