Command: |
RV.PATHLIST.CMDNUM |
---|---|
Command Syntax: |
RV.PATHLIST.CMDNUM |
Code |
Send "READ RV.PATHLIST.CMDNUM" |
Range: |
N/A |
Describe: |
READ RV.PATHLIST.CMDNUM - returns a list of command numbers for the path
|
Result: |
Return list of commands used to travel to the current way-point entry. 0 - Start of Way-points (if first action is a STAY, then no START is given, but a STAY will be shown instead.) 1 - Travel forward 2 - Travel backward 3 - Left spin motion 4 - Right spin motion 5 - Left turn motion 6 - Right turn motion 7 - Stay (no motion) the time the RV stays at the current position is given in the TIME list. 8 - RV is currently in motion on this way-point traversal. |
Type or |
Returns Data |