When using the Input and Output ports:
Certain I/O Modules require external power, as they use the 5V (OUT3 or IN3) ports on the TI-Innovator™ Hub. See the I/O Module section for details.
When using the Breadboard connector:
A circuit that is powered from the 5V output of the breadboard connector will require external power.