THERMISTOR i [TO] IN n/BB n

Command:

THERMISTOR i [TO] IN n/BB n

Command Syntax:

CONNECT THERMISTOR i [TO] IN n/BB n

Range:

 

Describe:

Connects a PTC thermistor to the system using a single analog input pin. The thermistor sensor uses the following values in the Steinhart-Hart model to convert the reading into a temperature.

Description

Value

C1

1.33342e-7

C2

2.22468e-4

C3

1.02119e-3

R1 – reference resistance

15000.0 ohms

CONNECT THERMISTOR i [TO] IN 1

CONNECT THERMISTOR i [TO] BB 5

Result:

Analog thermistor.

Type or
Addressable Component:

Sensor

THERMISTOR Data Sheet