| Module 13 - Implicit Differentiation | ||||||||||||||||||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Self-Test | ||||||||||||||||||||||||||||||||||||
| Lesson 13.1: Graphs of Implicit Relations | ||||||||||||||||||||||||||||||||||||
|
This lesson investigates graphing implicit relations. The expression x3 + y3 9xy = 0 implies a relation between x and y but the relation may not be obvious. A graph will help to illustrate the relation. Graphing an Implicit Relation The TI-89 can graph an implicit relation that has two variables x and y, but the Graph mode needs to be set properly. Setting the Mode
Entering the Relation In FUNCTION graphing mode, you define a set of functions of the form y(x), such as y1, but in 3D Graph mode, each function has the form z(x, y). That is, z is a function of two variables x and y and the graph of the function is a surface in three-space. When the Graph mode is 3D the names of the functions shown in the Y= Editor are z1, z2, etc. On the TI-89, an implicit relation is graphed by plotting all the points where z(x, y) = 0. The relation under consideration is x3 + y3 9xy = 0 , so let z = x3 + y3 9xy.
Setting the Graph Format Have the calculator display the axes, which are probably turned off in the 3D graphing mode.
Selecting Implicit Plot Style
Setting the Viewing Cube Values For 3D graphs the Viewing Window is called the Viewing Cube, and it is defined by the values of xmin, xmax, ymin, ymax, zmin, and zmax. The viewing angle is determined by the three components shown below.
eye
eye
eye The three viewing angle components are always entered as DEGREE measures regardless of the currently selected Angle mode. Setting the three viewing angle components as shown below displays the graph of the implicit relation as seen from above the xy - plane with the x- and y- axis in the standard orientation on the screen. Whenever one changes into IMPLICIT PLOT mode, the three viewing angles are set to these values automatically.
Be patient. It will take a minute or two for the graph to appear.
This graph is called a folium. It dates to Descartes in 1638.
13.1.1 Find the points on the graph of x3 + y3 9xy = 0 when x = 4 by using the solve command. |
||||||||||||||||||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||||||||||||||||||