Python ti_hub Module
As it appears in the CE Graphing Calculators
[Fns…]>Modul: ti_hub module
The ti_hub module contains the low-level command interfaces to send commands directly to the TI-Innovator™ Hub. The tables below show the function and command interfaces provided by this module.
Command: |
from ti_hub import * |
---|---|
Command Syntax: |
from ti_hub import * |
Method: |
|
Describe: |
Imports all methods from the ti_hub module. Note: When creating a new program that uses this module, it is recommended to use the Hub Project program type. This will ensure that all the relevant modules are imported. |
Result: |
|
Error: |
|
Type or |
|
Commands for from ti_hub import*
|
CE Calculators
|
TI‑Nspire™ CX
|