Errors

When the TI-34 MultiView™ calculator detects an error, it returns an error message with the type of error.

To correct the error, note the error type and determine the cause of the error. If you cannot recognize the error, use the following list, which describes error messages in detail.

Press - to clear the error message. The previous screen is displayed with the cursor at or near the error location. Correct the expression.

ARGUMENT — A function does not have the correct number of arguments.

DIVIDE BY 0 — You attempted to divide by 0.

DOMAIN — You specified an argument to a function outside the valid range. For example:

• For xÑy: x = 0 or (y < 0 and x is not an odd integer).
• For Ñx: x < 0.
• For LOG or LN: x { 0.
• For tan: x = 90Ä, -90Ä, 270Ä, -270Ä, 450Ä, etc., and equivalent for radian mode.
• For sin-1 or cos-1: |x| > 1.
• For nCr or nPr: n or r are not integers | 0.
• For }: Entering a simplify value of 0; using a simplify value of | 1¯10; attempting to simplify non-fractions.

EQUATION LENGTH — An entry exceeds the digit limits (88 for entry line and 47 for stat entries or constant entries); for example, combining an entry with a constant that exceeds the limit.

FRQ DOMAIN — FRQ value (in 1-var statistics) < 0.

OVERFLOW — You attempted to enter, or you have calculated, a number that is beyond the range of the calculator.

STAT — Attempting to calculate 1-var or 2-var stats with no defined data points, or attempting to calculate 2-var stats when the data lists are not of equal length.

CONVERSION

• The conversion does not contain a list name (L1, L2, or L3) followed by a conversion (for example, f³´d).
• You attempted to enter a function (for example, L1 + 3).

SYNTAX — The command contains a syntax error, or has misplaced functions, arguments, parentheses, or commas. If using P, try using W.

OP NOT DEFINED — Operation (op1 or op2) is not defined.

MEMORY LIMIT

• The calculation contains too many pending operations (more than 23).
• If using op1 or op2, you attempted to enter more than four levels of nested functions using fractions, square roots, exponents with ^, xÑ, and x2 (MathPrint™ mode only).

LOW BATTERY — Replace the battery

Note: This message displays briefly and then disappears. Pressing - does not clear this message.