Battery Information

Battery precautions

• Do not leave batteries within the reach of children.
• Do not mix new and used batteries. Do not mix brands (or types within brands) of batteries.
• Do not mix rechargeable and non-rechargeable batteries.
• Install batteries according to polarity (+ and -) diagrams.
• Do not place non-rechargeable batteries in a battery recharger.
• Properly dispose of used batteries immediately.
• Do not incinerate or dismantle batteries.
• Seek medical advice immediately if a cell or battery has been swallowed. In the USA, contact the National Capital Poison Center collect at 1-800-222-1222.

Battery disposal

Do not mutilate, puncture, or dispose of batteries in fire. The batteries can burst or explode, releasing hazardous chemicals. Discard used batteries according to local regulations.

Per CA Regulation 22 CCR 67384.4, the following applies to the button cell battery in this unit:

Perchlorate Material - Special handling may apply.

See www.dtsc.ca.gov/hazardouswaste/perchlorate

How to remove or replace the battery

The TI-34 MultiView™ calculator uses one 3 volt CR2032 lithium battery.

Remove the protective cover and turn the TI-34 MultiView calculator face downwards.

• With a small screwdriver, remove the screws from the back of the case.
• From the bottom, carefully separate the front from the back. Be careful not to damage any of the internal parts.
• With a small screwdriver (if required), remove the battery.
• To replace the battery, check the polarity (+ and -) and slide in a new battery. Press firmly to snap the new battery into place.

Important: When replacing the battery, avoid any contact with the other components of the TI-34 MultiView calculator.

Dispose of the dead battery immediately and in accordance with local regulations.