Angle Menu

% =

% = displays the choice of two submenus that enable you to specify the angle unit modifier as degrees (°), minutes ('), seconds ("), radian (r), or convert units using 44DMS. You can also convert between rectangular coordinate form (R) and polar coordinate form (P).

Choose an angle mode from the mode screen. You can choose from DEG (default) or RAD. Entries are interpreted and results displayed according to the angle mode setting without needing to enter an angle unit modifier.

If you specify an angle unit modifier from the Angle menu, the calculation is performed in that angle type, but the result will be given in the angle mode setting.

Examples

RAD

q " <

 

- % B 1

30 % = 1 E <

DEG

q <

¡ ¢ £

- 2 g % = 4 <

4DMS

1.5 % = 5 <

Convert polar coordinates (r,q)=(5,30) into rectangular coordinates. Then convert rectangular coordinates (x,y) = (3,4) into polar coordinates. Round the results to one decimal place.

R³´P

- q $ $ " " <

 

- % = " 3

5 % ` 30 E <

% = " 4

5 % ` 30 E <

 

% = " 1

3 % ` 4 E <

% = " 2

3 % ` 4 E <

Converting (r,q) = (5,30) gives (x,y) = (4.3,2.5) and converting
(x,y) = (3,4) gives (r,q) = (5.0,53.1).

³ Problem

Two adjacent angles measure 12Ä 31Å 45Æ and 26Ä 54Å 38 Æ respectively. Add the two angles and display the result in DMS format. Round the results to two decimal places.

- q $ $ " " " <

- 12 % =

1

31 % = 2

45 % = 3 T 26 % = 1

54 % = 2

38 % = 3 <

% = 5 <

The result is 39 degrees, 26 minutes and 23 seconds.

³ Problem

It is known that 30Ä = À / 6 radians. In the default mode, degrees, find the sine of 30Ä. Then set the calculator to radian mode and calculate the sine of À / 6 radians.

Note: Press - to clear the screen between problems.

- % B 1

30 E <

q " < -

% B 1 g P 6 " E <

Retain radian mode on the calculator and calculate the sine of 30¡. Change the calculator to degree mode and find the sine of À / 6 radians.

% B 1

30 % = < E <

q < -

% B 1 g P 6 " % = 4

E <