Parts of the TI-SmartView™ Emulator Workspace

Menu Bar - Use these menus to perform all emulator functions, including:

• File - exit or quit
• Actions - such as screen capture
• Edit - include copy key as font
• Help - Help and links
• View - change the displays

 

Note: You can complete most of the actions in these menus by clicking icons in the toolbar.

Toolbar- Use these toolbar icons to:

• Select a different calculator model
• Toggle displays of Large Display Screen hide or show, and Key Press History on or off
• Capture current emulator screen

Choose Emulator and Tool Bar Positions

• Emulator position Left/Right - to switch between left and right hand display of the scientific calculator screen. This is convenient when projecting on an Interactive White Board.
• Tool Bar Top/Bottom - to toggle the tool bar between the top and the bottom of the screen. This is convenient when projecting on an Interactive White Board.

Note: You can change the visual layout and/or position of elements to optimize access especially when using an Interactive White Board.

Emulator Panel - Use this panel to display the full emulator or the emulator keypad only view.

Large Display Screen Panel/Key Press History Panel - Use this panel to display a large version of the calculator screen and/or to display key press history.

You have the following display options:

• Large Display Screen only
• Key Press History only
• Large Display Screen + Key Press History
• Hide Large Display Screen

Resize Panels - Click and drag the vertical bar at the side of a panel to resize it.