Copying the Key Press History to Another Application

You can copy all or only a selected portion of the key press history to another application such as a word processor. You can copy the key graphics as they are shown in the key press history panel, or you can copy the key presses as font text characters 2 U 3.

Note: When you copy keys as font text characters, only primary key fonts paste. Second key fonts do not paste from the copy as font feature in TI-SmartView™. You can manually insert second features using the installed font. This font is installed on your computer automatically when you install the TI- SmartView™ for MathPrint™ calculators software.

Topic Links

Copying Keys as Graphics or Font Characters

1. Select the key(s) you want to copy.
To select keys in the Key Press History panel, use one of the following methods:

Key

Method

– A single key:

Click on a key.

– Multiple keys:

Click on a key.
Press and hold Ctrl on your computer keyboard.
Click other keys to select multiple keys.

– Multiple keys in a sequence:

Click on a key.

Press and hold Shift on your computer keyboard.

Press another key.

Note: This allows you to select those two keys plus all of the keys in between them.

– All keys:

Click on a key.
Right click.
Click Select All.

 

Note: This is what a key looks like before and after you select it.

Before:

After:

2. Select keys
3. Click Edit>Copy (to copy keys as graphics)

or

Click Edit>Copy As Font (to copy keys as the primary font character) 2 U 3.

4. Switch to another application.
5. Paste the keys at the appropriate location.

Note:

• You can also drag the selected keys as graphics to the other application.
• You can re-size the key graphics after you paste them into a new application.
• In some applications, the characters pasted as a font may be shown in the font that is in effect at that location, so they may not look anything like scientific calculator keys. If necessary, apply the appropriate calculator key font to the characters. See the help file for the destination application you are using for details on how to apply a font to the characters.