Data Editor and List Formulas

v

v lets you enter data in up to 3 lists. Each list can contain up to 42 items. Press % # to go to the top of a list, and % $ to go to the bottom of a list.

List formulas accept all calculator functions.

Numeric notation, decimal notation, and angle modes affect the display of an element (except fractional elements).

Example

L1

v 1 q 4 $ 2 q 4 $ 3 q 4 $ 4q 4 <

Formula

" v "

 

<

 

v < % j

 

<

Notice L2 is calculated per the formula you entered, and L2(1)= in the author line is highlighted to indicate the list is the result of a formula.

³ Problem

On a November day, a weather report on the Internet listed the following temperatures.

Paris, France 8°C

Moscow, Russia -1°C

Montreal, Canada 4°C

Convert these temperatures from degrees Celsius to degrees Fahrenheit.

Reminder: F = C + 32

v v 4

v " 5

8 $ M 1 $ 4 $ "

v " 1

9 W 5 V v 1 T 32

<

If Sydney, Australia is 21°C, find the temperature in degrees Fahrenheit.

! $ $ $ 21 <