Constant

% l

% l turns Constant feature on and lets you define a constant.

To store an operation to K and recall it:

1. Press % l.
2. Enter any combination of numbers, operators, and/or values, up to 44 characters.
3. Press < to save the operation. K displays in the indicator line.
4. Each subsequent time you press <, the TI-30XS MultiView™ calculator recalls the stored operation and applies it to the last answer or the current entry.

Press % l again to turn Constant feature off.

Examples

K

% l

 

V 2 T 3 <

 

4 <

 

6 <

Reset K

% l % l - F <

 

5 <

 

20 <

Turn off K

% l 1 T 1 <

³ Problem

Given the linear function y = 5x – 2, calculate y for the following values of x: -5; -1.

% l V 5 U 2 <

M 5 <

M 1 <

% l