Statistics Input Descriptions

The following table describes the different inputs used in Lists & Spreadsheet wizards.

Input

Description

m0

Hypothesized value of the population mean that you are testing.

s

The known population standard deviation; must be a real number > 0.

List

The name of the list containing the data you are testing.

Frequency List

The name of the list containing the frequency values for the data in List. Default=1. All elements must be integers | 0. The frequency values can also be typed as a list, in the format {1, 1, 3, 2}.

v, Sx, n

Summary statistics (mean, standard deviation, and sample size) for the one-sample tests and intervals.

s1

The known population standard deviation from the first population for the two-sample tests and intervals. Must be a real number > 0.

s2

The known population standard deviation from the second population for the two-sample tests and intervals. Must be a real number > 0.

List 1, List 2

The names of the lists containing the data you are testing for the two-sample tests and intervals.

Frequency 1, Frequency 2

The names of the lists containing the frequencies for the data in List 1 and List 2 for the two-sample tests and intervals. Defaults=1. All elements must be integers | 0.

v1, Sx1, n1,
v2, Sx2, n2

Summary statistics (mean, standard deviation, and sample size) for sample one and sample two in two-sample tests and intervals.

Pooled

Specifies whether variances are to be pooled for 2-Sample t Test and 2-Sample t Interval.

p0

The expected sample proportion for 1-Prop z Test. Must be a real number, such that 0 < p0 < 1.

x

The count of successes in the sample for the 1-Prop z Test and 1-Prop z Interval. Must be an integer | 0.

n

The count of observations in the sample for the 1-Prop z Test and 1-Prop z Interval. Must be an integer > 0.

x1

The count of successes from sample one for the 2-Prop z Test and 2-Prop z Interval. Must be an integer | 0.

x2

The count of successes from sample two for the 2-Prop z Test and 2-Prop z Interval. Must be an integer | 0.

n1

The count of observations in sample one for the 2-Prop z Test and 2-Prop z Interval. Must be an integer > 0.

n2

The count of observations in sample two for the 2-Prop z Test and 2-Prop z Interval. Must be an integer > 0.

C-Level

The confidence level for the interval instructions. Must be | 0 and < 100. If it is | 1, it is assumed to be given as a percent and is divided by 100. Default=0.95.

RegEQ

The prompt for the name of the function where the calculated regression equation is to be stored.