19.1.3
momentForCircle
inertia = physics.misc.momentForCircle(mass, innerRadius,
outerRadius, offBody)
|
Parameter |
Type |
Description |
|---|---|---|
|
mass |
in number |
The mass of the circle |
|
innerRadius |
in number |
The inner radius of the circle |
|
outerRadius |
in number |
The outer radius of the circle |
|
offset |
in physics.Vect |
The offset of the circle from the center of gravity |
|
inertia |
out number |
The inertia of the circle |
This
routine computes the moment of inertia for a circle.
A solid circle has an inner radius of 0. This is a useful helper routine for
computing the moment of inertia as an input to the physics.Body(...)
constructor.
Introduced in platform.apiLevel = '2.0'