19.4.31
sleep
self = physics.Body:sleep()
|
Parameter |
Type |
Description |
|---|---|---|
|
self |
in physics.Body |
The input Body |
|
bool |
out physics.Body |
The input Body is returned as the output |
Puts the Body to sleep.
Info
See http://chipmunk-physics.net/release/Chipmunk-5.x/Chipmunk-5.3.4-Docs/ for an explanation of sleeping bodies.
Note
The body must be added to a Space before it can be put to sleep.
Calling this function within a query or callback is not allowed.
Introduced in platform.apiLevel = '2.0'