6.1
set
cursor.set(cursorname)
Parameter cursorname is a string that contains the name of the cursor shape to use for the mouse pointer. It can be one of the following strings:
|
Cursor icon |
Cursor name |
SmartClick? |
Usage Notes |
|---|---|---|---|
|
|
"default", "pointer" |
N |
Used to show the position of the cursor. |
|
|
“hand pointer” |
Y |
Used to indicate that the underlying object can be selected or activated with a click. |
|
|
“crosshair” |
Y |
Used for fine control of a selection – often used to indicate the bounds of a rectangular region selection. |
|
|
'hand open" |
Y |
Indicates that the underlying object can be grabbed. |
|
|
"hand closed" |
N |
Indicates that the underlying object has been grabbed. |
|
|
"drag grab" |
N |
Typically used to indicate that a pan type of operation is in progress. |
|
|
“rotation” |
Y |
Indicates that the underlying object can be rotated and is also used to indicate that the rotation operation is ongoing. |
|
|
“translation” |
Y |
Indicates that the underlying object can be translated and is also used to indicate that the translation operation is ongoing. |
|
|
"dilation" |
Y |
Indicates that the underlying object can be dilated and is also used to indicate that the dilation operation is ongoing. |
|
|
“diag resize” |
Y |
Indicates that a grab at this location will initiate a diagonal resize operation. A hand closed should be used during the resize operation. |
|
|
“resize column” |
Y |
Indicates that a grab at this location will initiate a resize column or horizontal resize operation. A hand closed should be used during the resize operation. |
|
|
“resize row” |
Y |
Indicates that a grab at this location will initiate a resize row or vertical resize operation. A hand closed should be used during the resize operation. |
|
|
“zoom in” |
Y |
Indicates that a click will result in a zoom in. |
|
|
“zoom out” |
Y |
Indicates that a click will result in a zoom out. |
|
|
“zoom box” |
Y |
Indicates that a click will initiate a zoom box operation. |
|
|
"pencil" |
Y |
Indicates that a click will result in the next step in some kind of construction or drawing operation. |
|
|
"hide" |
Y |
Indicates that a click will hide the underlying object. |
|
|
"show" |
N |
Indicates that a click will show the underlying object. |
|
|
"clear" |
N |
Indicates that a click will delete the underlying object. |
|
|
"animate |
Y |
Indicates that a click will animate the underlying object. |
|
|
"interrogate" |
N |
|
|
|
"text" |
N |
Indicates that the underlying object is text and that a click will initiate an edit of that text. |
|
|
"link select" |
N |
Used as part of a linking operation to indicate that the underlying object is available to be linked to. |
|
|
"unavailable" |
N |
The current operation is unavailable for the underlying object. |
|
|
"wait busy" |
N |
Used by the system to indicate that the handheld is busy doing work. |
|
|
"writing" |
N |
Deprecated. |
|
|
"hollow pointer" |
Y |
Used when you need a SmartClick mouse pointer. Indicates that the object under the cursor can be selected. |
|
|
"arrow" |
N |
No standard usage. |
|
|
"dotted arrow" |
Y |
No standard usage. |
|
|
"excel plus" |
Y |
Used to indicate the location suitable for initiation of a drag to fill operation. |
|
|
"mod label" |
Y |
Deprecated. |
What is SmartClick?
| • | SmartClick improves the user experience by making it easier to center click on an object. |
How does it work?
| • | When the application displays a SmartClick cursor it is an indication that the next user operation will likely be a center click. Therefore, when a SmartClick cursor is displayed, any click (button press) on the touchpad will result in a center click event being sent to the active application. In this context the user does not have to worry about positioning the finger in the very center of the touchpad – even clicking on the edge of the touchpad will result in a center click. |
Introduced in platform.apiLevel = '1.0'