connect
error = peripheral:connect([timeout, ]callback [, object])
Requests connection to the Bluetooth® LE device represented by the peripheral object. The callback will be called for all events related to the connection state of this peripheral object. An optional timeout can be provided to automatically abort the request after the time specified. After disconnecting or after a failure during the connection procedure, the specified callback will not be referenced anymore.
Caution
Please make sure you disconnect peripheral objects before closing the document. A simple way to do so is by calling peripheral:disconnect() from the on.destroy() event.
|
Parameter |
Type |
Description |
|---|---|---|
|
timeout |
in number |
If provided, connection request
aborts after the specified time in seconds. |
|
callback |
in function |
Callback to receive asynchronous events about the connection state |
|
object |
out any (optional) |
If an object is provided it will be passed as the first parameter to the specified callback function. The object can be of any type except nil |
|
error |
out string (optional) |
If successful nil is returned, an error message otherwise |
Introduced in platform.apiLevel = '2.5'
Extended in platform.apiLevel = ‘2.6'
Callback Function
callback([object,] peripheral, event [, error])
The callback function provided in peripheral:connect() will be called
for every event related to the connection state between the Bluetooth
® LE central and the peripheral. Based on
whether
an object was provided in the call to connectPeripheral, the
callback should have three or four parameters.
|
Parameter |
Type |
Description |
|---|---|---|
|
object |
in any (optional) |
If an object was provided as a parameter to the function startScanning, it will be passed as the first parameter to this callback function |
|
peripheral |
in peripheral object |
A peripheral found during scanning |
|
event |
in bleCentral table constant |
Please see the following section for details |
|
error |
in string (optional) ) |
If successfully connected or disconnected
the |
Event Constants
The constants described in the following table are part of the bleCentral
table, e.g.
bleCentral.CONNECTED.
|
Name |
Description |
|---|---|
|
CONNECTED |
The connection has been successfully established |
|
CONNECTING FAILED |
The connect procedure failed. A new call of the connect() function is required to retry connecting. |
|
DISCONNECTED |
The connection has been successfully terminated |
Introduced in platform.apiLevel = '2.5'