Using a Displayed QR Code®

A QR Code® is an image that stores information, such as the address of a website or TI-Nspire™ document, as a pattern of small squares.


Web address http://education.ti.com stored as a QR Code®.

Authors of TI-Nspire™ documents can insert or paste a QR Code® on any Notes page. Users viewing the document with TI-Nspire™ App for iPad® can tell the app to scan the code directly from the page and link to its associated target. Lua scripts can also display a QR Code® that you can scan within the App.

Scanning a QR Code® on a Notes Page or Lua Script

Use this procedure to scan a displayed QR Code® and link to its target:

1. If necessary in Notes, scroll to ensure that only one code image is visible on your screen.

Note: The image must be entirely visible; the software will scan only the displayed region of the page.

2. Tap the Camera in the toolbar, and select Scan QR Code® from page.

- If the target is a TI-Nspire™ document (.tns file), the App automatically downloads the document, saves and closes your current document, and opens the downloaded document.
- Otherwise, the App opens your web browser to resolve the target.

How to Insert a QR Code® on a Notes Page

You can add QR Code® images to a Notes page. One image per page is best for reliable scanning.

1. Generate the image, using an online code generator or a code-generator app. You will need to supply the target URL.
2. Copy the generated image to the Clipboard, or save it as a photo.
3. Display your Notes page and use the method that applies for adding the image:
- If you copied the image to the Clipboard, press and hold the location on the page, and select Paste.
- If you saved the image as a photo, position the text cursor on the page, tap the Camera in the toolbar, and select Insert Photo.

The QR Code® appears on the Notes page with resizing handles.

Note: For optimal scanning, you should not resize or reshape the image.

4. (Optional) add a tip for users of your document who might not know how to use the code.

5. Make sure the code is valid by testing it with the Scan QR Code® from page feature.