What's New

What's New in TI-84 Plus CE-T Python

TI-84 Plus CE-T Python


OS

CE Calculator File Updates

• CE-T OS Update version v 5.8.0
- TI-84 Plus CE-T Python
- Supports TI Bluetooth Adapter
- TI-84 Plus CE-T
- OS update with minor fixes

OS Feature

CE OS Update to support TI Bluetooth® Adapter

• Detect and support TI Bluetooth® Adapter connection to Wonder Workshop Dash Robot


APPS

Setup App for Wonder Workshop Dash Robot

Note: Setup App is not included in the CE-T Bundle and is provided for download with the TI Python Dash activities.

• Calculator Name: SetDash
• Features include:
• List available Wonder Workshop Dash robots in range of the TI Bluetooth® Adapter.
• Name and store selected Dash robot in TI Bluetooth® Adapter memory for one time setup.
• After setup, Python App with ww_dash module is ready for you to program control the Dash robot.

Python App v5.7.1

• minor fixes

AppVars

Wonder Workshop Dash Robot programming with the TI Python experience

The following calculator files are included with TI Python Dash activities. These files are not included in the CE Bundle.

• Dash Add-On Module (AppVar)
• Add-On Module Name: wwi_dash
• "New Type" AppVar to support Python program templates for Dash activities
• AppVar name: WWD
• Use Dash program templates in the Python App to get started with Python programming the Dash robot.

TI-SmartView™ CE-T

• Emulator Workspace
- The CE-T emulator runs the Python App. To launch the Python App, select [prgm] 2:Python App.
• Explorer Workspace
- A Python program (PY AppVar) will save from the CE-T to a computer as *.py file. Open the *.py file in a text editor to view or edit the file for the CE Python experience. As in previous releases, TI-SmartView™ CE-T and TI Connect™ CE Explorer will send/convert .py files to the calculator file type, PY AppVar.
- When sending an image from a computer to the CE, an addition option to send/convert the file as a Python image (AppVar). Use the Python App and import the ti_image Add-On module to use your converted image in a program.

TI Connect™ CE

• Explorer Workspace additional Python file support
- A Python program (PY AppVar) will save from the CE to a computer as *.py file. Open the *.py file in a text editor to view or edit the file for the CE Python experience. As in previous releases, TI-SmartView™ CE and TI Connect™ CE Explorer will send/convert .py files to the calculator file type, PY AppVar.
- When sending an image from a computer to the CE, Explorer Workspace offers an additional option to send/convert the file as a Python image (AppVar). Then use the Python App and import the ti_image Add-On module to use your converted image in a Python program.

For more information about the new and updated functionality, go to education.ti.com/84cetupdate.