Using Setup App for Dash Robot Experience

Connecting a Dash robot to the TI Bluetooth® Adapter.

1. Load SetDash App on your CE calculator.
– Please update to the latest CE Bundle OS at education.ti.com/84cetupdate
– Load the SetDash App from education.ti.com/dash. The SetDash App is not included in the CE Bundle at this time.
2. Select one Bluetooth® Adapter/Dash robot from your classroom set of hardware.
3. Connect Adapter to CE.
– Use the Adapter to CE cable provided with your TI Bluetooth Adapter. The gray B side of the cable connects to the Adapter.
4. Turn on the Dash robot and CE calculator.
5. Run SetDash App in [apps] menu;
– Assume Adapter is detected.
– If the Adapter is not detected, detach one end of the cable and reattach. The screen will update with the status of the detected Adapter.

– If a Dash robot is stored in Adapter memory, the name, color and battery information display. You can change this information in [Menu] > 1:Edit Robot if needed.

– Select [Identify] for a head nod of the Dash robot currently connected to the Adapter. Here, Ingenuity will Identify with a head nod.

 

– If Adapter is not connected to a Dash robot OR a Dash robot is not available, follow the message on the screen. Use [Menu] options as directed.

– If Adapter is not detected, detach one end of the cable and reattach and follow updated screen message. The App screen will refresh and guide you to next steps.

 

6. Select [Menu] at f5

Menu choices are:

1: Search for Robots

– Displays a menu of all Dash robots powered on and in range of the TI Bluetooth® Adapter.

For simplicity and efficiency in classroom hardware set up, it is recommended that one Dash robot is turned on at a time to set up with one TI Bluetooth® Adapter.
However, the SELECT ROBOT menu will display up to 5 robots in range along with name, color and battery information.

 

2: Edit Robot Settings

– Edit Name and Color.
– Name: Edit the robot Name.
– Color: Use the right and left arrow keys to select a new color.
– Select "Done" to edit the robot setting.
– Select [Esc] to leave the screen with no update to the robot.

 

3: Forget This Robot

– Deletes the robot from Adapter memory.

 

4: Help

– How to setup the next Adapter and robot without leaving the App.

 

 

– How to take a screen capture of any screen in the App for your lessons.

 

5: Quit                  y 5

– Select [Esc] to remain in the App.
– Select [OK] to quit the App.

 

7. Once your class set of Dash robots and TI Bluetooth® Adapters are setup, please see the following to use CE Python with the Wonder Workshop Dash robot.

See: Python App Programming Guide

Learn more about Dash robots at www.makewonder.com