What's New
What's New in TI Connect™ CE Software
TI Connect™ CE
Send or Convert a Python AppVar to the Computer (*.py or *.8xv)
|
-
|
A Python program (PY AppVar) will save from the CE to a computer as *.py file. Open the *.py file in a text editor to view or edit the file for the CE Python experience. As in previous releases, TI-SmartView™ CE and TI Connect™ CE Explorer will send/convert *.py files to the calculator file type, PY AppVar. There is no need to save the CE PY AppVar on your computer. |
Convert an image for use in the Python App with the ti_image Add-On module
|
-
|
When sending an image from a computer to a connected CE, an additional image conversion option is available to convert and send the correct Python image AppVar format to the CE. Then, using the Python App, import the ti_image Add-On module to use the image in your program. |
Always update with the latest CE Bundle at: