Education Technology

Student On-line Courses

TI-Nspire™ CX II
and TI-Nspire™ CX II-T -
The Fundamentals


Please fill out your name and answer all 10 questions.
question 18 image

The page sorter view is displayed for a particular document. Identify all the applications used in the document:

Which key combination on the calculator is equivalent to a right mouse click (contextual menu) on a computer?

What keypad is pressed to view stored variables?

question 8 image

The calculator will not solve the simultaneous equations because

question 10 image

The user has just inserted a Data & Statistics application and the following message appears “No lists in this problem”, even though there is data in the Lists and Spreadsheet application. This is because

question 7 image

A graph is not shown for f1(x). This is because:

question 9 image

A box plot has been drawn in a Data and Statistics application from the data shown in the Lists and Spreadsheet application. In the data and statistics application, how do you add the second parallel box plot?

question 12 image

There are three graphs displayed in the Graphs application shown. The best way to see a table of values for all three graphs at the one time, is to press:

question 15 image

In the Graphs application, point A is on the curve f1(x)=x2. The coordinates of point A have been defined as (x1,y1). The coordinates of point P have been defined as: (x1 + 1,y1 – 4). Point A is moved to the origin. The coordinates of point P will now be:

question 14 image

A series of maths boxes have been set up in the Notes application such that a, b and c are the side lengths of a triangle. If the value of value of ‘a’ is changed to 9, which of the following values will update automatically?