Module 19 - Exponential Growth and Decay
 
  Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test
 
 Self Test
 

  1. How long will an investment take to double if it earns interest compounded continuously at an annual rate of 5%?
  2. How much will $5000 be worth in 25 years if it earns interest compounded continuously at 8%?
  3. For Questions 3 and 4: A cup of water was heated to a temperature of 90°. It was placed in a refrigerator that had a temperature of 11°C. The water cooled to a temperature of 17°C in 30 minutes.

  4. Find the value of k in the differential equation tL' = –k · (tLtS).
  5. Predict the temperature of the water in 60 minutes.
  6. For Questions 5 and 6: A capacitor discharges voltage such that v(0) = 8.9 and v(30) = 1.7.

  7. Find the value of k in the differential equation V' = kV
  8. Find the half-life of the capacitor.

Click here to check your answers.


< Back
  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy