| Module 19 - Exponential Growth and Decay |
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test |
| Lesson 19.3: Charge on a Capacitor |
|
A capacitor stores electrical energy that can be discharged quickly or slowly. For example, energy from a battery is stored in a camera's capacitor and then the voltage quickly discharges to create the bright flash of light created by a flash bulb. In this lesson you will examine data produced by a capacitor as it discharges. The discharge discussed is much slower than that of a flash bulb because an electronic resistor, which retards the discharge, was placed in the circuit with the capacitor. Finding the Voltage Equation When a capacitor discharges through a resistor, the voltage across the capacitor decreases at a rate proportional to the amount of remaining voltage. This is described by the differential equation V' = kV and V(0) = V0 where V represents the voltage across the capacitor at any time t, k is a negative parameter that depends on the physical characteristics of the capacitor and resistor, and V0 represents the capacitor's initial voltage. A Texas Instruments CBL and voltage probe were used to measure the discharge of energy from a capacitor. The design for this experiment is described in Real-World Math with the CBL-2 and LabPro, Activity 18, which is published by Texas Instruments and can be found in the Online Store at http://education.ti.com/us/product/book/rwmwb.html. The data from the capacitor experiment are stored in lists l1 and l2, which should be downloaded to your computer and calculator. Downloading the Data to Your Computer
Transferring the Data to the TI-89 Click here to get information about how to obtain the needed cable and to review the procedure to transfer the program from your computer to your calculator.
Time, measured in seconds, is in l1 and voltage, measured in volts, is in l2. Plotting the Data and Solving the Differential Equation
Each list can be found by pressing
The graph of the data in l1 and l2 shows a particular solution to the differential equation V' = kV and V(0) = V0.
The graph indicates that the initial voltage was V0
Solve the initial-value problem V' = kV and V(0) = 7.93407
Use another point on the graph to find the value of k.
The value of k can be found by solving V = 7.93407ekt with the values t = 30 and V = 2.0928.
Graph the function to see that the equation fits the original data well.
19.3.1 Trace on the scatter plot of the data to t = 50 and write down the corresponding value of v. Use this value of v to find a new value for k. How well does the solution to the differential equation using this value of k fit the original data? Finding Half-Life
19.3.2 Find the half-life of the capacitor by solving the equation
|
| < Back | Next > |
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|