Module 17 - Applications of Integration | |||||||||||||||||||||||||||||||||||||||||
Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | |||||||||||||||||||||||||||||||||||||||||
Lesson 17.1: Net Area | |||||||||||||||||||||||||||||||||||||||||
In previous modules you used the definite integral to find the area bounded by a function and the x-axis. In each case the graph of the function was above the x-axis. In this lesson you will see what happens when the function dips below the x-axis. You will also investigate the concept of the definite integral as a net area function. All the curves explored in Module 16 were above the x-axis and the net area functions were always positive and increasing. The following investigates a definite integral when part of the curve is below the x-axis.
![]()
![]()
How can the result be zero? The area bounded by y = sin x and the x-axis certainly is not zero. To help answer this question, break the interval of integration into two subintervals that represent the areas above and below the x-axis: (0,
![]() Finding Positive and Negative Integrals
Review the graph of y = sin x and the values of the definite integrals
![]() ![]()
The graph from 0 to
The graph from
Finding Net Area
The definite integral
17.1.1 Use the definite integral feature in the F5:Math menu of the Graph screen to approximate the values of
Click here for the answer.
Visualizing
You may obtain the general shape of a corresponding net area function on the interval [0, 2
![]()
The following characteristics of the net area function
Using the fact that
Other characteristics of the net area function include:
With these characteristics you can draw a graph of the net area function
Visualizing the general shape of the integral function
Extending the Procedure to Other Curves 17.1.2 Graph the curve and find the net area bounded by y = x3 – 3x2 – x + 3 and the x-axis on the interval [0, 4]. Click here for the answer.
Visualizing
The characteristics of the net area function
The graphs of the curve function and the net area function are shown below for comparison.
17.1.3 Approximate the graph of a net area function that corresponds to the following curve from 0 to 4. ![]() Click here for the answer. |
|||||||||||||||||||||||||||||||||||||||||
< Back | Next > | |||||||||||||||||||||||||||||||||||||||||
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|