Module 1 - Describing Functions | ||||||||||
Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Lesson 4 | Self-Test | ||||||||||
Lesson 1.1: Basic Features | ||||||||||
In this lesson you will reset the TI-89 to its factory default settings and adjust the calculator's contrast. Then you will learn how to go to the Home screen and you will learn about the four basic parts of the Home screen. Reset Default Factory Settings
To start fresh you should reset the calculator to its original factory settings. Note that the default command restores all system variables and modes to their original factory setting. It does not erase stored programs or user-defined variables. "Default" should be highlighted in the current menu, as shown below. Setting the Screen Contrast You can adjust the screen contrast by repeatedly pressing to darken the contrast or to make the contrast lighter. Notice is green. 1.1.1 What icon is printed in green beside the and keys? Click here for the answer. Note: The notation r.s.t stands for Module number r, lesson number s and question number t. Clearing the Home Screen Your calculator is probably already on the Home screen, but in case it is not, press . If the Home screen is not clear, you can erase its contents by pressing .
The Home Screen The Home screen is divided into several parts: the Toolbar, the History Area, the Edit Line, and the Status Line. The Toolbar, shown at the top of the Home screen, contains menus that can be selected by pressing the function keys through [F8]. Notice that [F6], [F7] and [F8] are noted in yellow above , , and , respectively. You will learn about these menus throughout this online course. The function of each key may vary depending on which screen is active. If you press a function key and then wish to back out of the menu, press . The central part of the Home screen is called the History Area. As you enter commands in the TI-89, you will see these commands and their results in the History Area. The rectangle below the History Area of the Home screen is called the Edit Line. This is where you will actually enter calculator commands. Beneath the Edit Line is the Status Line where you can see some of the current calculator settings. You will learn more about these settings during this online course. |
||||||||||
< Back | Next > | ||||||||||
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|