You are here: Graphs Application > Plotting Sequences

Plotting Sequences

The Graphs application lets you plot two types of sequences. Each type has a separate template for defining the sequence.

Defining a Sequence

1. From the Graph Entry/Edit menu, select Sequence > Sequence.

2. Type the expression to define the sequence.
3. Type an initial term. If the sequence expression references more than one prior term, such as u1(n‑1) and u1(n‑2), separate the terms with commas.

4. Press Enter.

Defining a Custom Sequence

A custom sequence plot shows the relationship between two sequences by plotting one on the x axis and the other on the y axis.

This example simulates the Predator-Prey model from biology.

1. Use the relations shown here to define two sequences: one for a rabbit population, and another for a fox population. Replace the default sequence names with rabbit and fox.

.05 = the growth rate of rabbits if there are no foxes
.001 = the rate at which foxes can kill rabbits
.0002 = the growth rate of foxes if there are rabbits
.03 = the death rate of foxes if there are no rabbits

Note: If you want to see the plots of the two sequences, zoom the window to the Zoom ‑ Fit setting.

2. From the Graph Entry/Edit menu, select Sequence > Custom.
3. Specify the rabbit and fox sequences to plot on the x and y axes, respectively.

4. Press Enter to create the custom plot.
5. Zoom the window to the Zoom ‑ Fit setting.

6. Explore the custom plot by dragging the point that represents the initial term.

 

© 2006 - 2016 Texas Instruments Incorporated