You are here: Using the TI‑SmartView™ Emulator > Using the Touchpad

Using the Touchpad

You can operate the Touchpad on the TI‑Nspire™ Touchpad keypad using either the touchpad on a laptop or by using the mouse to click the Touchpad. Areas of the Touchpad are highlighted as you click the arrow zones.


An arrow is highlighted when you press or tap it.

Clicking the ¡, ¢, £, or ¤ keys on the Touchpad moves through menus one item at a time.
Clicking and holding down an arrow on the Touchpad causes continual movement in the selected direction.
Clicking and sliding the mouse across the Touchpad area enables you to move the mouse pointer.
Clicking the middle of the Touchpad selects the highlighted menu option.

 

© 2006 - 2016 Texas Instruments Incorporated